Quadruped Robot Fire Rescue Solutions

Overcome Hazards

Protect the Ones Who March Against the Tide

Watch Video →
Intelligent Reconnaissance Modular Design
Deeply integrated into Fire Rescue industry applications, the product supports modular functions and replacements.
High performance of Stair-Climbing Capability
With high performance stair-climbing ability, it can effortlessly climb steep stairs.
For ascending and descending steps (facing front): the maximum height is 40cm, When climbing “fire stairs”, it has excellent stability and balance capabilities.
Drencher system
Ensures that the robot dog can continue to operate in high-temperature environments without being affected by heat, thus improving fire-extinguishing efficiency.
Qingdao Fire Department Officially Equips New Robots

Recently, two advanced quadruped robots have been officially added to the Qingdao Firefighting and Rescue Support Team, injecting new scientific and technological strength into Qingdao's firefighting and rescue work.

The deployment of these quadruped robots marks a significant step forward for the Qingdao Firefighting and Rescue Support Team in the modernization and intelligentization of firefighting equipment. It will greatly enhance the rescue capabilities and efficiency of the firefighting and rescue teams in complex environments, providing a solid guarantee for the protection of people's lives and property.

Quantity: 2 units

360 degree camera

dual-light cloud platform

self-network

gas sensor

industrial-grade remote controller

Injecting new scientific and technological strength into Qingdao's firefighting and rescue work.
Comprehensive Emergency Drill of Intelligent Equipment for Forest Fires

In the fire drill mission for forest fire prevention and extinguishing, water cannon robot dogs were used for fire inspection and fire-source location tasks. During the actual drill, fire rescue robot dogs were also deployed for post-disaster monitoring, constantly observing the fire-ground dynamics to ensure that the fire was completely extinguished without reignition risks. This demonstrates that fire rescue robot dogs play a crucial role not only in the fire-extinguishing process but also provide significant support in post-disaster management.

Quantity: 1 units + 1 units

360 degree camera

dual-light cloud platform

point-to-point communication

industrial-grade remote controller

water cannon

dual - light camera

point-to-point communication

industrial-grade remote controller

In the simulating a wild forest fire scene, with the theme of "monitoring, prevention, and extinguishing", robot dogs were used for reconnaissance and fire - extinguishing, demonstrating a new emergency rescue model of human - robot collaboration and efficient operation.
Comprehensive Live - fire Drill for Firefighting and Rescue in Large Commercial Complexes

The drill simulated a fire in a store on the underground commercial street of a commercial center, which was caused by an oil - fume pipeline catching fire. The reconnaissance robot dog climbed up via the mall's internal elevator and quickly conducted multi - level environmental reconnaissance on - site and coordinated with command decision - making.

Quantity: 1 unit

360 degree camera

dual-light cloud platform

gas sensor

point-to-point communication

industrial-grade remote controller

This drill fully simulated the real life fire and fire-ground handling environment, providing a comprehensive inspection of personnel, equipment, robot dogs, and tactical strategies.

Contact Us

  • Contact Team
    sales_global@unitree.cc
  • Contact Sales
    +86 15336583018

* The Inspection robot dog/ Water cannon robot dog/ Air blower robot dog are only sold to countries and regions that accept certain conditions.